Other Parts Discussed in Thread: F28M35H52C
Hi!
After reading all documentation and posts in this forum related to SPI interface and McBSP interface as SPI in C28 core of F28M35, I'm convinced that the TI only guarantees proper operation under the following maximum rates:
SPI Master
TX: 25 MHz
RX: 12.5 MHz
SPI Slave
TX: 12.5 MHz
RX: 12.5 MHz
McBSP as SPI Master
TX: 25 MHz
RX: 25 MHz
McBSP as SPI Slave
TX: 9.375 MHz
RX: 9.375 MHz
Regarding the last condition, the datasheet has the following information:
For all SPI slave modes, CLKX has to be minimum 8 CLKG cycles. Also CLKG should be LSPCLK/2 by setting CLKSM = CLKGDV = 1. With maximum LSPCLK speed of 75 MHz, CLKX maximum frequency will be LSPCLK/16 , that is 4.6875 MHz and P = 13.3 ns.
but I assume LSPCLK can reach 150 MHz, as stated in this same document and argued by AndyP in this discussion: https://e2e.ti.com/support/microcontrollers/c2000/f/171/p/291452/1016372
First of all, I would like to have some confirmation on these conclusions, for both F28M35H52C and F28M36P63C devices. Assuming they are correct, I would like to know if it's possible to have some information from the C2000 team about how exaclty these values were specified.
The reason I'm asking it is the fact we've been working with F28M35 in prototypes of digital controllers for switched mode power supplies for 2 years, using the SPI interface as slave receiving samples from an external ADC with transmission rates of 25 MHz, and we haven't experienced any problems up to now. Furthermore, we've made some tests to observe communication errors between two F28M35 development kits for all conditions above, with rates up to 18.75 MHz running continuously without any bit error.
At the end, I just would like to understand what exaclty TI (or any other manufacturer) means with specified limits like these. It sounds to me something like: "when working beyond these conditions, things might work (even for long periods), but we can't guarantee that a sporadic event due to 'working under improper conditions' won't occur". Is it correct?
Thanks in advance!
Gabriel Brunheira