Other Parts Discussed in Thread: TMS320F28035
In TMS320F28035 in the analog comparator, I am trying to use Ramp Generator input for the DAC.
The rampsource can be set to PWMSYNC1,2,3 and 4 only. If I use PWM5,PWM6,PWM7 then how should the RAMPSOURCE be specified ? So it means the RAMPSOURCE can not be synchronized with PWM5,PWM6 and PWM7. Am I right ?
Is it possible to use ramp generator with out using PWMSYNC ? From the statement in the spruge5f "The values of the RAMPMAXREF_SHDW shadow registers are copied to the active registers on the next PWMSYNC signal". So does it mean that RAMPMAXREF_SHDW cannot be updated in ISR dynamically with out using PWMSYNC.
I really appreciate your help in answering these questions.
Regards,
Srinath.