Other Parts Discussed in Thread: BOOSTXL-DRV8301, DRV8301
Hello,
I´m working with LAUNCHXL-F28027F combined with BOOSTXL-DRV8301 to get current measurement results, and on LAUNCHXL-F28027F I left Switch S4 on because I wanted to have communication with Scilab, and devices were working properly, but after some time I got this message:
C28xx: Flash Programmer: Warning: The configured device (TMS320F28027), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx: GEL Output:
Device Calibration not complete, check if device is unlocked and recalibrate.C28xx: GEL Output:
Device Calibration not complete, check if device is unlocked and recalibrate.C28xx: Flash Programmer: Device is locked or not connected. Operation cancelled.
C28xx: GEL: File: C:\Users\sdidovic\Desktop\Diplomski\LaunchPad\TI_TMS320F28027_LounchPad\Blinky.out: Load failed.
and since then I can´t establish Connection with LAUNCHXL-F28027F. Is the device damaged? And is the Problem that I left swich S4 turned on, because later I´ve read in datasheet that it should be turned off. And if that´s the case is there a way to use BOOSTXL-DRV8301with swich S4 turned on?
Thanks in advance,
Said