In the BUILD setting, found in the {ProjectName}-Settings.h file.Should we have to change the frequency to 50 Hz and voltage 220V as per indian standard.What are all the changes to be done in the settings?Could you please tell.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Depends on what build level you are using.. in build level3 it is auto detected by software.. so if you have 220V the freq qill be 50Hz and if you have 110Hz at the output the freq will be 60Hz
if you are in build level 2 and doing grid connect and testing just the inverter portion then you will need to change the values ..