Other Parts Discussed in Thread: BOOSTXL-DRV8301
I'm working on my own "boostxl-DRV8301" hardware. Occasionally I need to change something in the hardware, power it down, and then want to resume my program.
The program has been flashed into on-chip flash, so re-flashing is unnecessary. The only way I've found to get back my debugging session is to hit the green debug button, but that starts a compile-and-flash cycle that takes a lot of time. The compile is quick enough, but the flash is slowing me down. Can I reconnect to the target without reflashing?
Run->connect target gives me: "device blocked debug access because it is currently running non-debuggable code". Hitting the debug then tells me "allready running" and when I confirm it reflashes and works....
Is there a way to avoid the re-flash?