Hello Everyone!!
I recently try change from CCS3.3 to CCSCCS Version 6.1.0.00104 in windows 7 32bits
I used spectrum Digital XDS510 for TMS320F28335 board debugging with CCS3.3.
I guess XDS510 has no problem because it work well with CCS3.3.
And CCS Version 6.1.0.00104's installed without error message.
I programed one project and build it.
But can't debugging with XDS501 connection error.
I execute ti/ccsv6/ccs_base/emucation/specdig/sdconfiggex.
In SDConfigEx, select XDS510USB-PLUS with Default option.
Configuration tag shows like bellow
BUS : XDS510-USB
>> XDS510-USB Emulator not connected/enumerated
>> Could not open emulation connection
In Device management pain, XDS510 USB is shown with warn mark.
How to connect XDS510 USB on SDConfigEx and how to use SDConfigEx with CCS6?