Other Parts Discussed in Thread: CONTROLSUITE
Hi everybody, I'm trying to use the Flash API example found in the Control suite folder for the F28M35x devices. I've imported the project in CCS for both the M3 core and the C28 core. II've linked to the M3 example project the F021_API_CortexM3_LE.lib and the F021_Concerto_Cortex.h files (they are not included in the original example project, I was wondering why), but when i try to build the project, the compiler returns two times the error: "Could not open source file "F021_Concerto_Cortex.h"". The same thing happens with the C28 example project with the C_28 lib files included, which returns: "Could not open source file "F021_Concerto_C28x.h"". The files the compiler can not open are in the main folder of the same project.
Could someone help me please to understand what is going wrong? Thank you in advance
Best regards,
Filippo