This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

InstaSPIN for generator and max RPM

I have to develop a SRM control and I have basic knowledge of motors. The motor that I have to control is going to work like a generator also. Can I use InstaSPIN for this? 

The motor needs to work at almost 19000 RPM. Do you think that InstaSPIN is able to work properly at that speed?