This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the TMS320F28335 EPWM sync feature be used to synchronize timing on multiple F28335 devices or only modules on a single device? Please advise.
Thanks,
Mark
Mark,
In short: either and/or both.
Take a look at Figure 9 in the current version of the F2833x/F2823x ePWM User's Guide (SPRUG04a)
http://www.ti.com/lit/sprug04
As you'll see there, PWMs can be synched by external pulses (via EPWMSYNCI in the GPIO mux), a F2833x can output PWM1's synch pulse (via EPWMSYNCO in the GPIO mux), and/or you can synch one ePWM module to another ePWM module.
Hopefully this helps.
Thank you,
Brett