This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28062 GPIO39 Port is only switched to '1' if 2 times execute order



Dear All

I use GPIO39 as common output port.

Here my code:

 //       MOT2_ENA3 = 1;  //if I actvate this line then MOT2_ENA3 is '1'. without this line MOT2_ENA3 stay '0'
        if (SysPar.ui16FunctionBlockEnable & BIT_MOTOR_DISABLE)
        {
            MotDisablePwm(1);
            return;
        }
        MOT2_ENA1 = 1;
        MOT2_ENA2 = 1;
        MOT2_ENA3 = 1;
        MOT2_ENA4 = 1;
        MotPwmSetPh3A(EPwm1Regs.TBPRD >> 1);
        MotPwmSetPh3B(EPwm1Regs.TBPRD >> 1);
        MotPwmSetPh4A(EPwm1Regs.TBPRD >> 1);
        MotPwmSetPh4B(EPwm1Regs.TBPRD >> 1);
        EALLOW;
        GpioCtrlRegs.GPAMUX1.all |= 0x00005500; //Enable PWM3,4
        EDIS;
        Ui16MotEnable[1] = 1;

Here the definition's:


#define MOT2_ENA4                          GpioDataRegs.GPBDAT.bit.GPIO44
#define MOT2_ENA3                          GpioDataRegs.GPBDAT.bit.GPIO39
#define MOT2_ENA2                          GpioDataRegs.GPADAT.bit.GPIO26
#define MOT2_ENA1                          GpioDataRegs.GPBDAT.bit.GPIO43

Here the initialistion of these ports (Inside EALLOW and EDIS)
   GpioCtrlRegs.GPBDIR.all = 0x0000;      // GPIO32-GPIO63 are inputs
   GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;  //VREF_SPM2
   GpioCtrlRegs.GPBDIR.bit.GPIO39 = 1;  //MOT2_ENA3
   GpioCtrlRegs.GPBDIR.bit.GPIO43 = 1;  //MOT2_ENA1
   GpioCtrlRegs.GPBDIR.bit.GPIO44 = 1;  //MOT2_ENA4

Problem: GPIO34,43,44 are working well. GPIO39 is only '1' if I activate the first line of my code. (return (Line 2 -6) is not used in all cases of my test program.)

It seems to me the CPU need 2 times the same GPIO39-->'1' order. I also can set the port with emulator after execution of this program, and then it works also after setting with emulator (And we are sure no other process is disturbing). Or I execute GPIO39-->'1' order before or after this small program in the code. Then also it is working. Imortant is 2 times same GPIO39-->'1' order.

The output of port correspondent with the watch window of GpioDataRegs.GPBDAT register.

I checked also different settings compiler optimation. No difference in result.

Compiler: CCS 5.5.0.0077 Ti v6.2.5

I use a very small test SW with only this functionality.

Assembly code of ASM File (without any optimation)

;----------------------------------------------------------------------
; 299 | if (SysPar.ui16FunctionBlockEnable & BIT_MOTOR_DISABLE)                
;----------------------------------------------------------------------
        MOVW      DP,#_SysPar+3         ; [CPU_U]
        TBIT      @_SysPar+3,#0         ; [CPU_] |299|
        BF        $C$L9,NTC             ; [CPU_] |299|
        ; branchcc occurs ; [] |299|
    .dwpsn    file "C:/Eigene_Dateien_D/projekte/SmartOptionII/Software/Sandbox/source/motor_pwm.c",line 301,column 7,is_stmt
;----------------------------------------------------------------------
; 301 | MotDisablePwm(1);                                                      
;----------------------------------------------------------------------
        MOVB      AL,#1                 ; [CPU_] |301|
$C$DW$41    .dwtag  DW_TAG_TI_branch
    .dwattr $C$DW$41, DW_AT_low_pc(0x00)
    .dwattr $C$DW$41, DW_AT_name("_MotDisablePwm")
    .dwattr $C$DW$41, DW_AT_TI_call
        LCR       #_MotDisablePwm       ; [CPU_] |301|
        ; call occurs [#_MotDisablePwm] ; [] |301|
    .dwpsn    file "C:/Eigene_Dateien_D/projekte/SmartOptionII/Software/Sandbox/source/motor_pwm.c",line 302,column 7,is_stmt
;----------------------------------------------------------------------
; 302 | return;                                                                
;----------------------------------------------------------------------
        B         $C$L10,UNC            ; [CPU_] |302|
        ; branch occurs ; [] |302|
$C$L9:    
    .dwpsn    file "C:/Eigene_Dateien_D/projekte/SmartOptionII/Software/Sandbox/source/motor_pwm.c",line 304,column 6,is_stmt
;----------------------------------------------------------------------
; 304 | MOT2_ENA1 = 1;                                                         
;----------------------------------------------------------------------
        MOVW      DP,#_GpioDataRegs+8   ; [CPU_U]
        OR        @_GpioDataRegs+8,#0x0800 ; [CPU_] |304|
    .dwpsn    file "C:/Eigene_Dateien_D/projekte/SmartOptionII/Software/Sandbox/source/motor_pwm.c",line 305,column 6,is_stmt
;----------------------------------------------------------------------
; 305 | MOT2_ENA2 = 1;                                                         
;----------------------------------------------------------------------
        OR        @_GpioDataRegs+1,#0x0400 ; [CPU_] |305|
    .dwpsn    file "C:/Eigene_Dateien_D/projekte/SmartOptionII/Software/Sandbox/source/motor_pwm.c",line 306,column 6,is_stmt
;----------------------------------------------------------------------
; 306 | MOT2_ENA3 = 1;                                                         
;----------------------------------------------------------------------
        OR        @_GpioDataRegs+8,#0x0080 ; [CPU_] |306|
    .dwpsn    file "C:/Eigene_Dateien_D/projekte/SmartOptionII/Software/Sandbox/source/motor_pwm.c",line 307,column 6,is_stmt
;----------------------------------------------------------------------
; 307 | MOT2_ENA4 = 1;                                                         
;----------------------------------------------------------------------
        OR        @_GpioDataRegs+8,#0x1000 ; [CPU_] |307|
    .dwpsn    file "C:/Eigene_Dateien_D/projekte/SmartOptionII/Software/Sandbox/source/motor_pwm.c",line 308,column 6,is_stmt
;----------------------------------------------------------------------
; 308 | MotPwmSetPh3A(EPwm1Regs.TBPRD >> 1);                                   
;----------------------------------------------------------------------
        MOVW      DP,#_EPwm1Regs+5      ; [CPU_U]
        MOV       AL,@_EPwm1Regs+5      ; [CPU_] |308|
        MOVW      DP,#_EPwm3Regs+9      ; [CPU_U]
        LSR       AL,1                  ; [CPU_] |308|
        MOV       @_EPwm3Regs+9,AL      ; [CPU_] |308|
    .dwpsn    file "C:/Eigene_Dateien_D/projekte/SmartOptionII/Software/Sandbox/source/motor_pwm.c",line 309,column 6,is_stmt
;----------------------------------------------------------------------
; 309 | MotPwmSetPh3B(EPwm1Regs.TBPRD >> 1);                                   
;----------------------------------------------------------------------


Where is the problem?

Best regards and thank you for any ideas.

Franz