This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compute Back EMF



 

Dear Sirs,

 

In manual spruhj1f, Page 411 Figure 11-19, Decoupled PI Controllers for a PMSM

 

Vq = PID_q_out + id * ω * Ls + ω * KE ;

 

 

I want to use “USER_MOTOR_RATED_FLUX * ω(rad/s) * 2 * 3.1415 “to substitute for “ω * KE”, is it right

 

If I use ω * KE Vpeak/KPRM, do I need to use

“ω(KPRM) * KE / (PolePaires * sqrt(3))” or others?

 

I am not sure. Please Help.

 

Thanks a lot.

 

  • Hello Mingjiang Li,
    The second term (w*KE) accounts for the back-emf voltage, which is the largest component of the compensation voltage term in most cases. The equation assumes KE is in units of peak volts, line-to-neutral per electrical radians/second, and speed is in units of electrical radians/seconds. If you use a KE or speed value in any other units, you must correct the scaling to get it back to these units.
    Let's take a look at your example. Since USER_MOTOR_RATED_FLUX is in units of Volts/Hz, you must convert it to Volts per radian per second. To do this, you need to DIVIDE by 2*pi, not multiply by it.
    If you use w*KE (Vpeak/KRPM), then you once again need to convert KE to the correct units. If Vpeak is line-to-line (it's not clear from your comments), then you need to convert it to line-to-neutral. To convert from KRPM to electrical radians/sec, you need to multiply by 1000*pole-pairs*2*pi/60.
    Hope that helps,Dave
  • Dave,

       Thanks for your response. This solve my problems.

       Really appreciate.