I am using internal temperature sensor for tmperature measurement
I am using control suite example of adc_temp_seso_conv
It measures temperature and converts to degree
I had executed the sample code
1. I am seeing 47 degrees as tmperature in watch window of CCS and it is fluctuating However, the ambient air temperature is 32 degree.
2. If I am using internal oscillator with temperature compensation . How reliable it is compared to external oscillator which has variation of 50ppm i.e 0.0005% variation.
3. Also internal oscillator has variation of +- 0.1 MHZ for variation of +-10 degree. SO I was proposing to use temperature compensation , While it is showing 47 degeree for ambinet of 32 degree.