This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI Communication with FPGA

I am using F28M35 Concerto which is communicating with FPGA on SPI bus(4- wire)(Mode 0). Can you tell me the maximum frequency at which full duplex communication can be done ? I have set LSPCLK to 75 MHz. At this case I am receiving data in my fpga correctly ( @ 18.75MHz which is maximum possible SPICLK in this case )  but Concerto misses one bit. I am little bit of confusede why it is happening. What is the maximum frequency at which Concerto can receive and transmits the data to any device on SPI slave ? Waiting reply urgently !

Regards,

Akshay