This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C Interrupt in MotorWare

Other Parts Discussed in Thread: MOTORWARE

Hi there,

I'm trying to use I2C to control two LAUNCHXL-F28069Ms. As far as I can see, communication works fine until the PWMs start at which point the I2C gets borked. The weird part is this communication only gets messed up when both motors are on and both boards are connected to the I2C bus. Has anyone successfully implemented I2C in a motorware project? Does anyone have any idea why this could be happening?

Thanks so much,
Ben

EDIT: is it possible that it could be an electrical problem? Enough noise on the I2C bus when there are two motors running but not one?