Other Parts Discussed in Thread: SN74ACT244
Hello!
All GPIO PINS in F28335 (but not gpio0-11 (EPWM)) have an internal pullup if XRSn line is low (and after reset). In my application i need that some GPIO lines have a low level during reset (these GPIO pins connect to input of SN74ACT244). I want to use the external pulldown resistor 3.3 kohm. Value of 3.3 kohm of pulldown resistor if sufficient to drive the gpio line to low level or not?
P.S. Epwm pins are used in this application for other purposes.
Sorry for my english.