This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does "LM Flash Programmer" still support USB interface (DFU)?

Expert 1960 points

Other Parts Discussed in Thread: CONTROLSUITE, UNIFLASH

Hi there,

I downloaded the latest release of "LM Flash Programmer" from TI website, and tried to use it to load my app into F28069 Piccolo device. But somehow the USB DFU option is not listed on Interface box anymore. The built-in help document still has  a whole section about USB bootloading, and shows a screenshot with USBDFU interface selected. But it's not listed or selectable from the software. Any idea why? I do have the latest USB bootloader installed and running in the Piccolo device, and was able to use a simple cmd-line utility (dfuprog) to write an example app into device flash. THe TI USB bootloader manual says that you can use either dfuprog or "LM Flash Programmer" to program. But do I get the LM Flash PRogrammer to work? Thanks!