This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Has anyone got C2Prog work with USB DFU interface?

Expert 1960 points
Other Parts Discussed in Thread: CONTROLSUITE

Hi,

I want to use C2Prog to program a small app into F28069 controlCard. I've built, loaded and tested USB bootloaded in the Piccolo device with dfuprog. But somehow C2Prog does not work when seleting USB DFU. It just waits there forever after I pressed "program" button. Any one has any idea what could be wrong? Thanks!

  • Hi Shef,

    Here's the reference, did you follow the same:

    Regards,

    Gautam

  • Hi again,
    Yes I did follow the steps in the manual and have the TI USB bootloader installed on my 28069U, and tested from dfuprog successfully. But I'm nto sure how to verify WinUSB GUID. I installed the Windows driver from the controlSuite v141 for f2806x. If this is nto good enough, where should I get the correct version? Thanks again Gautam! You are always so helpful.