Hi,
I am using CCS 6.1.0 and controlsuite 3.3.2.
Board i am using is F2837x control card R1.1.
Initially there was connection problems randomly, but right now it is not getting connected in any manner. Even in the device manager there is XDS 100 connected.
When i am staring debug an error message is getting pop uped like below:
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during
the connect returned bad status or an error.
The cause may be one or more of: invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
Also there is some heat in the controller too. Please advice.
Regards,
Anish