Other Parts Discussed in Thread: CONTROLSUITE, TMDSCNCD28069ISO
Hi there,
I'm very new to this TI Launchxl F28069m. I'm trying to find the example of using usb communication, but do not find one. However, I've found the example of usb_dev_bulk for F28069m but not directly for this launchpad. I successfully compile and download the code to the board and connect the usb port from computer to the pin D-, D+ at the pin GPIO27, GPIO26 respectively and issue the command line "usb_bulk_example" but the program can't start because tiusbdll.dll is missing. I think the usb driver "usb_dev_bulk_x86.inf" is not installed. My questions are follows:
1. Do I need the Vbus for this particular example? or just D- D+ are okay?
2. How to install "usb_dev_bulk_x86.inf" ?
Hope any expert can help me on this, thanks.
Veerachai