Other Parts Discussed in Thread: TMS320F2811, CONTROLSUITE
Hello,
I have been trying to flash my application via serial port for TMS320F2811 device like given in the example
http://www.ti.com/lit/an/spraaq2/spraaq2.pdf
Currently, I am using the CKFA code modified for F2811 device and trying to flash via the hyperterminal from my PC. I am able to boot from UART and send data via serial port to Boot ROM and tried transferring CKFA.bin as given in the example and it works..it asked for relocking baudrate and erase flash and after erasing flash, I transferred the AppCode.bin given for 128kW to check if the application is getting programmed and it successfully completed and showed application programmed.
I tried to do the same procedure for my existing software application .out file which i flash with JTAG normally. The .out file and .map file, I rename them to AppCode.out and .map as given in the example and run the batch file given in the example to generate .bin file for F2811 device. Now CKFA gets loaded properly and when i start transferring my new .bin file, the application programming starts normally and keeps giving the "." as progress and after some time...it does not end and it just stays without giving any error and does not show application programmed, I have removed cheksum verification since the expected checksum by the CKFA code will be different now.
I am attaching a picture of hyperterminal where it stops.
I am unable to figure it how it works for the sample application and not for my application, Is there any specific changes required in CKFA code like increasing RAM size or buffer size, does it stop because of that?? Please suggest