Other Parts Discussed in Thread: UNIFLASH, TMS320F2811
After much messing about it seems that Uniflash works very nicely with a JTAG emulator (the Spectrum Digital 510USB), but I can’t make it work with the serial connection, although it did get a lot further than yesterday, complaining “C28xx: Can't Initialize Target CPU: Error starting communication transport: 2147500037”.
Also, the serial connection doesn’t work as an emulator either, giving the messages: C28xx: Flash Programmer: Warning: The configured device (TMS320F2811), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx: GEL: Error while executing OnTargetConnect(): Could not read register ST1: Execution state prevented access at (ST1&~(0x0100)) [f2811.gel:254] at C28x_Mode() [f2811.gel:76] at OnTargetConnect() .
C28xx: Failed CPU Reset: Unsupported GTI Function.
From these opaque messages and the TI documentation it looks like the serial connection doesn’t work with the F2811 for UniFlash.
Please could you confirm whether the serial connection should work with the F2811 & UniFlash.