This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to calculate Period register for 100Hz.



Hi guys,

    How to calculate the EPWM1_TIMER_TBPRD (Period register for 100Hz).

   Thanks in advance.

  • Hi Sachin,

    Your ePWM is in Up or Down or UP-Down count mode?

    Regards,
    Gautam
  • Here's for both:

  • Hi gautam,
    I have got this code from the forum for a switching frequency of 2050.2Hz , If i change the period register for 100Hz then my program will run for 100Hz switching frequency or i need to change anything else.
    #include <stdio.h>
    #include <file.h>

    #include "DSP28x_Project.h" // DSP28x Headerfile
    #include "f2802x_common/include/F2802x_GlobalPrototypes.h"

    #include "f2802x_common/include/pll.h"
    #include "f2802x_common/include/clk.h"
    #include "f2802x_common/include/wdog.h"

    #include "f2802x_common/include/flash.h"
    #include "f2802x_common/include/gpio.h"
    #include "f2802x_common/include/pie.h"
    #include "f2802x_common/include/adc.h"
    #include "f2802x_common/include/sci.h"
    #include "f2802x_common/include/sci_io.h"
    #include "f2802x_common/include/pwm.h"
    #include "f2802x_common/include/timer.h"
    #include "f2802x_common/include/IQmathLib.h" //IQmath Library header file


    extern void DSP28x_usDelay(Uint32 Count);
    #pragma DATA_SECTION(sine_table,"IQmathTables"); //IQmath ROM sine table
    _iq30 sine_table[512];


    //Interrupt prototype function for timer0
    interrupt void cpu_timer0_isr(void);
    void update_compare(void);

    //Global PWM variables
    #define EPWM1_TIMER_TBPRD 14634 // Period register for 2050.2Hz
    #define PHASE 120.0 // Defines the real in degrees phase between phases, 120deg
    #define TTIMERREG 2343 // Timer interrupt for 50Hz SPWM
    Uint16 EPWM_PHASE=(EPWM1_TIMER_TBPRD*PHASE/180.0); //The phase as seen from the EPWM module
    Uint16 duty_cycle_A=1000; // Set duty 50% initially
    Uint16 duty_cycle_B=1000; // Set duty 50% initially
    Uint16 index=0;
    Uint16 DEADTIME_R=5.0;
    Uint16 DEADTIME_F=5.0;
    Uint16 y=0.0;


    // Handles setup
    CPU_Handle myCpu;
    PLL_Handle myPll;
    WDOG_Handle myWDog;
    CLK_Handle myClk;
    ADC_Handle myAdc;
    FLASH_Handle myFlash;
    GPIO_Handle myGpio;
    PIE_Handle myPie;
    SCI_Handle mySci;
    PWM_Handle PWMA,PWMB,PWMC;
    TIMER_Handle myTimer0;


    // Handles initialization
    void setup_handles()
    {

    myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj));
    myPll = PLL_init((void *)PLL_BASE_ADDR, sizeof(PLL_Obj));
    myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj));
    myCpu = CPU_init((void *)NULL, sizeof(CPU_Obj));

    myFlash = FLASH_init((void *)FLASH_BASE_ADDR, sizeof(FLASH_Obj));
    myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj));
    myPie = PIE_init((void *)PIE_BASE_ADDR, sizeof(PIE_Obj));
    mySci = SCI_init((void *)SCIA_BASE_ADDR, sizeof(SCI_Obj));
    myAdc = ADC_init((void *)ADC_BASE_ADDR, sizeof(ADC_Obj));
    PWMA = PWM_init((void *)PWM_ePWM1_BASE_ADDR, sizeof(PWM_Obj));
    PWMB = PWM_init((void *)PWM_ePWM2_BASE_ADDR, sizeof(PWM_Obj));
    PWMC = PWM_init((void *)PWM_ePWM3_BASE_ADDR, sizeof(PWM_Obj));
    myTimer0 = TIMER_init((void *)TIMER0_BASE_ADDR, sizeof(TIMER_Obj));

    }

    //System Initialization
    void init_system()
    {
    //Disable watchcdog
    WDOG_disable(myWDog);
    //Device calibration for the adc
    (*Device_cal)();
    //Sets the internal oscillator source
    CLK_setOscSrc(myClk, CLK_OscSrc_Internal);

    // Setup the PLL for x10 /2 which will yield 60Mhz = 10Mhz * 12 / 2
    PLL_setup(myPll, PLL_Multiplier_12, PLL_DivideSelect_ClkIn_by_2);

    //Disable the PIE peripheral and all the interupts
    PIE_disable(myPie);
    PIE_disableAllInts(myPie);
    CPU_disableGlobalInts(myCpu);
    CPU_clearIntFlags(myCpu);

    #ifdef _FLASH
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
    #endif
    }

    //GPIO initialization
    void gpio_init()
    {
    // Initialize GPIO for the EPWM1A and EPWM1B
    GPIO_setPullUp(myGpio, GPIO_Number_0, GPIO_PullUp_Disable);
    GPIO_setPullUp(myGpio, GPIO_Number_1, GPIO_PullUp_Disable);
    GPIO_setMode(myGpio, GPIO_Number_0, GPIO_0_Mode_EPWM1A);
    GPIO_setMode(myGpio, GPIO_Number_1, GPIO_1_Mode_EPWM1B);
    GPIO_setDirection(myGpio,GPIO_Number_0,GPIO_Direction_Output);
    GPIO_setDirection(myGpio,GPIO_Number_1,GPIO_Direction_Output);

    // Initialize GPIO for the EPWM2A and EPWM2B
    GPIO_setPullUp(myGpio, GPIO_Number_2, GPIO_PullUp_Disable);
    GPIO_setPullUp(myGpio, GPIO_Number_3, GPIO_PullUp_Disable);
    GPIO_setMode(myGpio, GPIO_Number_2, GPIO_2_Mode_EPWM2A);
    GPIO_setMode(myGpio, GPIO_Number_3, GPIO_3_Mode_EPWM2B);
    GPIO_setDirection(myGpio,GPIO_Number_2,GPIO_Direction_Output);
    GPIO_setDirection(myGpio,GPIO_Number_3,GPIO_Direction_Output);

    // Initialize GPIO for the EPWM2A and EPWM2B
    GPIO_setPullUp(myGpio, GPIO_Number_4, GPIO_PullUp_Disable);
    GPIO_setPullUp(myGpio, GPIO_Number_5, GPIO_PullUp_Disable);
    GPIO_setMode(myGpio, GPIO_Number_4, GPIO_4_Mode_EPWM3A);
    GPIO_setMode(myGpio, GPIO_Number_5, GPIO_5_Mode_EPWM3B);
    GPIO_setDirection(myGpio,GPIO_Number_4,GPIO_Direction_Output);
    GPIO_setDirection(myGpio,GPIO_Number_5,GPIO_Direction_Output);
    }

    //PWM settings
    void pwma_init()
    {

    // PWMA initialization
    CLK_enablePwmClock(myClk, PWM_Number_1);

    //PWMA initialiazation

    // Setup TBCLK
    PWM_setCounterMode(PWMA,PWM_CounterMode_UpDown); // Count up-down
    PWM_setPeriod(PWMA,EPWM1_TIMER_TBPRD); // Set timer period
    PWM_disableCounterLoad(PWMA); // Disable phase loading
    PWM_setSyncMode(PWMA,PWM_SyncMode_CounterEqualZero);
    PWM_setPhase(PWMA,0x0000); // Phase is 0
    PWM_setCount(PWMA, 0x0000); // Clear counter
    PWM_setClkDiv(PWMA, PWM_ClkDiv_by_1);
    PWM_setHighSpeedClkDiv(PWMA, PWM_HspClkDiv_by_1); // Clock ratio to SYSCLKOUT

    // Setup shadowing
    PWM_setShadowMode_CmpA(PWMA, PWM_ShadowMode_Shadow);
    PWM_setShadowMode_CmpB(PWMA, PWM_ShadowMode_Shadow);
    PWM_setLoadMode_CmpA(PWMA, PWM_LoadMode_Zero);
    PWM_setLoadMode_CmpB(PWMA, PWM_LoadMode_Zero);

    PWM_setCmpA(PWMA,1000); //Initial duty cycle
    PWM_setCmpB(PWMA,1000);

    // Set actions
    PWM_setActionQual_CntUp_CmpA_PwmA(PWMA, PWM_ActionQual_Set); // Set PWM1A on event A, up count
    PWM_setActionQual_CntDown_CmpA_PwmA(PWMA, PWM_ActionQual_Clear); // Clear PWM1A on event A, down count
    PWM_setActionQual_CntUp_CmpB_PwmB(PWMA, PWM_ActionQual_Clear); // Set PWM1B on event B, up count
    PWM_setActionQual_CntDown_CmpB_PwmB(PWMA, PWM_ActionQual_Set); // Clear PWM1B on event B, down count

    //Set DeadBand Control
    PWM_setDeadBandOutputMode(PWMA, PWM_DeadBandOutputMode_EPWMxA_Rising_EPWMxB_Falling);
    PWM_setDeadBandPolarity(PWMA, PWM_DeadBandPolarity_EPWMxB_Inverted);
    PWM_setDeadBandInputMode(PWMA, PWM_DeadBandInputMode_EPWMxA_Rising_and_Falling);
    PWM_setDeadBandRisingEdgeDelay(PWMA, DEADTIME_R);
    PWM_setDeadBandFallingEdgeDelay(PWMA, DEADTIME_F);
    //--------------------------------------------------------------------------------------------------------------------
    //--------------------------------------------------------------------------------------------------------------------

    //PWMB initialization

    CLK_enablePwmClock(myClk, PWM_Number_2);

    // Setup TBCLK
    PWM_setCounterMode(PWMB,PWM_CounterMode_UpDown); // Count up-down
    PWM_setPeriod(PWMB,EPWM1_TIMER_TBPRD); // Set timer period
    PWM_enableCounterLoad(PWMB);
    PWM_setPhaseDir(PWMB,PWM_PhaseDir_CountDown);
    PWM_setSyncMode(PWMB,PWM_SyncMode_EPWMxSYNC);
    PWM_setPhase(PWMB,EPWM_PHASE); // Phase is 120 degrees
    PWM_setCount(PWMB, 0x0000); // Clear counter
    PWM_setClkDiv(PWMB, PWM_ClkDiv_by_1);
    PWM_setHighSpeedClkDiv(PWMB, PWM_HspClkDiv_by_1); // Clock ratio to SYSCLKOUT

    // Setup shadowing
    PWM_setShadowMode_CmpA(PWMB, PWM_ShadowMode_Shadow);
    PWM_setShadowMode_CmpB(PWMB, PWM_ShadowMode_Shadow);
    PWM_setLoadMode_CmpA(PWMB, PWM_LoadMode_Zero);
    PWM_setLoadMode_CmpB(PWMB, PWM_LoadMode_Zero);

    PWM_setCmpA(PWMB,1000); //Initial duty cycle
    PWM_setCmpB(PWMB,1000);

    // Set actions
    PWM_setActionQual_CntUp_CmpA_PwmA(PWMB, PWM_ActionQual_Set); // Set PWM2A on event A, up count
    PWM_setActionQual_CntDown_CmpA_PwmA(PWMB, PWM_ActionQual_Clear); // Clear PWM2A on event A, down count
    PWM_setActionQual_CntUp_CmpB_PwmB(PWMB, PWM_ActionQual_Clear); // Set PWM2B on event B, up count
    PWM_setActionQual_CntDown_CmpB_PwmB(PWMB, PWM_ActionQual_Set); // Clear PWM2B on event B, down count

    //Set DeadBand Control
    PWM_setDeadBandOutputMode(PWMB, PWM_DeadBandOutputMode_EPWMxA_Rising_EPWMxB_Falling);
    PWM_setDeadBandPolarity(PWMB, PWM_DeadBandPolarity_EPWMxB_Inverted);
    PWM_setDeadBandInputMode(PWMB, PWM_DeadBandInputMode_EPWMxA_Rising_and_Falling);
    PWM_setDeadBandRisingEdgeDelay(PWMB, DEADTIME_R);
    PWM_setDeadBandFallingEdgeDelay(PWMB, DEADTIME_F);
    //---------------------------------------------------------------------------------------------------------------
    //---------------------------------------------------------------------------------------------------------------

    //PWMC initialization

    CLK_enablePwmClock(myClk, PWM_Number_3);

    // Setup TBCLK
    PWM_setCounterMode(PWMC,PWM_CounterMode_UpDown); // Count up-down
    PWM_setPeriod(PWMC,EPWM1_TIMER_TBPRD); // Set timer period
    PWM_enableCounterLoad(PWMC);
    PWM_setPhaseDir(PWMC,PWM_PhaseDir_CountUp);
    PWM_setSyncMode(PWMC,PWM_SyncMode_EPWMxSYNC);
    PWM_setPhase(PWMC,EPWM_PHASE); // Phase is 120
    PWM_setCount(PWMC, 0x0000); // Clear counter
    PWM_setClkDiv(PWMC, PWM_ClkDiv_by_1);
    PWM_setHighSpeedClkDiv(PWMC, PWM_HspClkDiv_by_1); // Clock ratio to SYSCLKOUT

    // Setup shadowing
    PWM_setShadowMode_CmpA(PWMC, PWM_ShadowMode_Shadow);
    PWM_setShadowMode_CmpB(PWMC, PWM_ShadowMode_Shadow);
    PWM_setLoadMode_CmpA(PWMC, PWM_LoadMode_Zero);
    PWM_setLoadMode_CmpB(PWMC, PWM_LoadMode_Zero);

    PWM_setCmpA(PWMC,1000); //Initial duty cycle
    PWM_setCmpB(PWMC,1000);

    // Set actions
    PWM_setActionQual_CntUp_CmpA_PwmA(PWMC, PWM_ActionQual_Set); // Set PWM3A on event A, up count
    PWM_setActionQual_CntDown_CmpA_PwmA(PWMC, PWM_ActionQual_Clear); // Clear PWM3A on event A, down count
    PWM_setActionQual_CntUp_CmpB_PwmB(PWMC, PWM_ActionQual_Clear); // Set PWM3B on event B, up count
    PWM_setActionQual_CntDown_CmpB_PwmB(PWMC, PWM_ActionQual_Set); // Clear PWM3B on event B, down count

    //Set DeadBand Control
    PWM_setDeadBandOutputMode(PWMC, PWM_DeadBandOutputMode_EPWMxA_Rising_EPWMxB_Falling);
    PWM_setDeadBandPolarity(PWMC, PWM_DeadBandPolarity_EPWMxB_Inverted);
    PWM_setDeadBandInputMode(PWMC, PWM_DeadBandInputMode_EPWMxA_Rising_and_Falling);
    PWM_setDeadBandRisingEdgeDelay(PWMC, DEADTIME_R);
    PWM_setDeadBandFallingEdgeDelay(PWMC, DEADTIME_F);

    CLK_enableTbClockSync(myClk);
    }

    //PIE settings
    void pie_init()
    {
    PIE_enable(myPie);
    EALLOW;
    EDIS;
    PIE_registerPieIntHandler(myPie, PIE_GroupNumber_1, PIE_SubGroupNumber_7, (intVec_t)&cpu_timer0_isr);
    EDIS;
    }

    //Timer settings
    void timer0_init()
    {
    TIMER_stop(myTimer0);
    TIMER_setPeriod(myTimer0,TTIMERREG);
    TIMER_setPreScaler(myTimer0,0);
    TIMER_reload(myTimer0);
    TIMER_setEmulationMode(myTimer0, TIMER_EmulationMode_StopAfterNextDecrement);
    TIMER_enableInt(myTimer0);
    TIMER_start(myTimer0);
    }

    void main()
    {

    setup_handles();
    init_system();
    gpio_init();
    pwma_init();
    pie_init();
    timer0_init();

    //Enables the CPU interrupt
    CPU_enableInt(myCpu, CPU_IntNumber_1);
    //Enables the interrupt of the Timer0 for the PIE module
    PIE_enableTimer0Int(myPie);
    CPU_enableGlobalInts(myCpu);
    CPU_enableDebugInt(myCpu);



    //Forever Loop to see the results
    for(;;)

    {

    }
    }

    interrupt void cpu_timer0_isr(void)
    {
    update_compare();

    // Acknowledge this interrupt to receive more interrupts from group 1
    PIE_clearInt(myPie, PIE_GroupNumber_1);
    }

    void update_compare(void)
    {
    PWM_setCmpA(PWMA,_IQsat(_IQ30mpy((sine_table[index]+_IQ30(0.9999))/2,EPWM1_TIMER_TBPRD),EPWM1_TIMER_TBPRD,0));
    PWM_setCmpB(PWMA,_IQsat(_IQ30mpy((sine_table[index]+_IQ30(0.9999))/2,EPWM1_TIMER_TBPRD),EPWM1_TIMER_TBPRD,0));
    PWM_setCmpA(PWMB,_IQsat(_IQ30mpy((sine_table[index]+_IQ30(0.9999))/2,EPWM1_TIMER_TBPRD),EPWM1_TIMER_TBPRD,0));
    PWM_setCmpB(PWMB,_IQsat(_IQ30mpy((sine_table[index]+_IQ30(0.9999))/2,EPWM1_TIMER_TBPRD),EPWM1_TIMER_TBPRD,0));
    PWM_setCmpA(PWMC,_IQsat(_IQ30mpy((sine_table[index]+_IQ30(0.9999))/2,EPWM1_TIMER_TBPRD),EPWM1_TIMER_TBPRD,0));
    PWM_setCmpB(PWMC,_IQsat(_IQ30mpy((sine_table[index]+_IQ30(0.9999))/2,EPWM1_TIMER_TBPRD),EPWM1_TIMER_TBPRD,0));

    if (index++ >511) index = 0;
    }
  • do some math, what is the clock_rate of your system? what PWM freq do you need? Look again the figure 6 in Gautam post.
  • I need a PWM freq of 100Hz and do be frank i haven't understood the program fully as i m having very less time to understand the whole program so can u plz explain me in sort it will be very helpfull.
  • TBclk is the prescaled version of the SYSCLKOUT. What is the CPU rate of your system? 60Mhz? 90Mhz? Ex: I want Fpwm = 1Kh (Tpwm = 1/1Khz) for PWM, then if my Clock Rate is 60Mhz (TBclk), employing the above formulas) the Tpwm = 59999.
    regards
    Gastón
  • I forgot to mention this value is what you put in the TBPRD register.
    Regards