Other Parts Discussed in Thread: CONTROLSUITE
hi
i am using E50S8-1024-6-L-5 rotary encoder with 1024 ppr and have signals A B Z with line driver output of 5v connecting to a Texas Instruments DSP processor (TMS32028335 ).I go thorugh the the code given in the: ti\controlSUITE\libs\device_support\f2833x\v132\DSP2833x_examples_ccsv4...
1)i can connect A B Z Signals to the qep module of processor right. with pins(5V A B Z Gnd)?
2) how can i convert 5v signals to 3.3 v before connecting to a dsp? should i initailise or configure any thing else in tms32028335 dsp processor codings?
3)When i am using a floating point processor should i change any program of position speed calculations...in this program there are some lines with IQ MATH LIB...is that needed for a floating point processor..
eg:
if (newp>oldp)
Tmp1=-(_IQ(1)-newp+oldp)?etc
Hope u can answer my queris..it would be grateful if you could help me regarding the same......thanking you in advance
Regards
Joseph