This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue with enmeration of F2806x with USB

Hi,

We are using a F2806x on a  customized board and connecting the same to the SBC via USB.

The USB on the F2806x is configured as a device. The class used is Vendor Specifice Class.

The issue is: If I connect the USB device to the PC/Laptop the enumeration is completed and I can talk to the device over USB.

But, If I connect the same to the SBC, the enueration fails (When debugged the device is in suspended state).. If I reset the host, then the enmeration is complete.

Another case is: If I connect to the PC and then connect to the SBC, the enumeration is complete.

I have tested with different power sources and different power sequencing, the result does not change.

2 out of 10 boards of device had it working in the first attempt. 8 have the issue of enumeration not completed.

Can anyone please help me understand the issue.