Hi All
I am searching a good DC power line solution for autonomous home appliance application, "DC Power LIne Communication Reference design" is a good example but with many sub boards.
Here I only need one -to -one the first stage, I have 3 question:
1 System on Module for PRIME Power Line Communication (CENELEC Frequency Band) is a one-board PLC SOM, Does it can be easily used in DC 24V PLC with around 8A Bus current.
How should I modify the board if it's ok.
2. DC Power LIne Communication Reference design was designed for multi node LED application, If I want to reuse it to the big current scenery as above, what I need to modify.
3. Where to buy the demo kits.
thank you and best regards
Eric