This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Memory allocation on TMS320F28035

I used a program in FLASH with PRAGMA for parts of program who need to run faster. This seems to be ok.
It worked well but if I want to add just one variable (int Info = 0 ) as global then I have to following ERROR message.



Description Resource Path Location Type

#10010 errors encountered during linking; "tempo.out" not built tempo C/C++ Problem


Description Resource Path Location Type

<a href="file:/G:/ti/ccsv5/tools/compiler/dmed/HTML/10099.html">#10099-D</a> program will

not fit into available memory. placement with alignment/blocking fails for section ".text" size .0x2006 page 0. Available memory ranges: F28035.cmd /tempo/cmd line 122 C/C++ Problem

I used CCS5 (Version: 5.5.0.00077) and there is optimization 4 "Whole program optimizations" in

compilation option.

 

to be able to compile en execute the program i changed standard CMD file such as :


   /* Allocate program areas: */
   .cinit              : >  FLASHA | FLASHC | FLASHD,      PAGE = 0
   .pinit              : >  FLASHA | FLASHC | FLASHD,      PAGE = 0
   .text               : >  FLASHA | FLASHC | FLASHD,      PAGE = 0
   codestart           : > BEGIN       PAGE = 0
   ramfuncs            : LOAD = FLASHF,

It seems the there is no more place in the flash to store the code but the code is not so big !

Is that possible to know the real percentage of flash used by the code in the CPU using CCS5, It will be very helpful ??


thanks for your help

here under CMD file

 

/*
// TI File $Revision: /main/4 $
// Checkin $Date: November 9, 2009   15:09:12 $
//###########################################################################
//
// FILE:    F2808.cmd
//
// TITLE:    Linker Command File For F2808 Device
//
//###########################################################################
// $TI Release: 2803x C/C++ Header Files V1.21 $
// $Release Date: December 1, 2009 $
//###########################################################################
*/
 
/* ======================================================
// For Code Composer Studio V2.2 and later
// ---------------------------------------
// In addition to this memory linker command file,
// add the header linker command file directly to the project.
// The header linker command file is required to link the
// peripheral structures to the proper locations within
// the memory map.
//
// The header linker files are found in <base>\DSP2803x_Headers\cmd
//
// For BIOS applications add:      DSP2803x_Headers_BIOS.cmd
// For nonBIOS applications add:   DSP2803x_Headers_nonBIOS.cmd
========================================================= */
 
/* ======================================================
// For Code Composer Studio prior to V2.2
// --------------------------------------
// 1) Use one of the following -l statements to include the
// header linker command file in the project. The header linker
// file is required to link the peripheral structures to the proper
// locations within the memory map                                    */
 
/* Uncomment this line to include file only for non-BIOS applications */
/* -l DSP2803x_Headers_nonBIOS.cmd */
 
/* Uncomment this line to include file only for BIOS applications */
/* -l DSP2803x_Headers_BIOS.cmd */
 
/* 2) In your project add the path to <base>\DSP2803x_headers\cmd to the
   library search path under project->build options, linker tab,
   library search path (-i).
/*========================================================= */
 
/* Define the memory block start/length for the F28035
   PAGE 0 will be used to organize program sections
   PAGE 1 will be used to organize data sections
 
   Notes:
         Memory blocks on F2803x are uniform (ie same
         physical memory) in both PAGE 0 and PAGE 1.
         That is the same memory region should not be
         defined for both PAGE 0 and PAGE 1.
         Doing so will result in corruption of program
         and/or data.
 
         L0 memory block is mirrored - that is
         it can be accessed in high memory or low memory.
         For simplicity only one instance is used in this
         linker file.
 
         Contiguous SARAM memory blocks or flash sectors can be
         be combined if required to create a larger memory block.
*/
 
MEMORY
{
PAGE 0:    /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
   RAML0       : origin = 0x008000, length = 0x000800     /* on-chip RAM block L0 */
   RAML1       : origin = 0x008800, length = 0x000400     /* on-chip RAM block L1 */
   OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
   FLASHH      : origin = 0x3E8000, length = 0x002000     /* on-chip FLASH */
   FLASHG      : origin = 0x3EA000, length = 0x002000     /* on-chip FLASH */
   FLASHF      : origin = 0x3EC000, length = 0x002000     /* on-chip FLASH */
   FLASHE      : origin = 0x3EE000, length = 0x002000     /* on-chip FLASH */
   FLASHD      : origin = 0x3F0000, length = 0x002000     /* on-chip FLASH */
   FLASHC      : origin = 0x3F2000, length = 0x002000     /* on-chip FLASH */
   FLASHA      : origin = 0x3F6000, length = 0x001F80     /* on-chip FLASH */
   CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
   CSM_PWL_P0  : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
 
   IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
   IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
   IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA      /* IQ Math Tables in Boot ROM */
 
   ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
 
PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */
   BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
   RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
   RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAML2       : origin = 0x008C00, length = 0x000400     /* on-chip RAM block L2 */
   RAML3       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L3 */
   FLASHB      : origin = 0x3F4000, length = 0x002000     /* on-chip FLASH */
 
}
 
/* Allocate sections to memory blocks.
   Note:
         codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
                   execution when booting to flash
         ramfuncs  user defined section to store functions that will be copied from Flash into RAM
*/
 
SECTIONS
{
 
   /* Allocate program areas: */
   .cinit              : >  FLASHA | FLASHC | FLASHD,      PAGE = 0
   .pinit              : >  FLASHA | FLASHC | FLASHD,      PAGE = 0
   .text               : >  FLASHA | FLASHC | FLASHD,      PAGE = 0
   codestart           : > BEGIN       PAGE = 0
   ramfuncs            : LOAD = FLASHF,
                         RUN = RAML0,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         PAGE = 0
 
   csmpasswds          : > CSM_PWL_P0  PAGE = 0
   csm_rsvd            : > CSM_RSVD    PAGE = 0
 
   /* Allocate uninitalized data sections: */
   .stack              : > RAMM0       PAGE = 1
   .ebss               : > RAML2       PAGE = 1
   .esysmem            : > RAML2       PAGE = 1
 
   /* Initalized sections go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst             : > FLASHA      PAGE = 0
   .switch             : > FLASHA      PAGE = 0
 
   /* Allocate IQ math areas: */
   IQmath              : > FLASHA      PAGE = 0            /* Math Code */
   IQmathTables        : > IQTABLES,   PAGE = 0, TYPE = NOLOAD
 
  /* Uncomment the section below if calling the IQNexp() or IQexp()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {
 
              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
 
   }
   */
    /* Uncomment the section below if calling the IQNasin() or IQasin()
       functions from the IQMath.lib library in order to utilize the
       relevant IQ Math table in Boot ROM (This saves space and Boot ROM
       is 1 wait-state). If this section is not uncommented, IQmathTables2
       will be loaded into other memory (SARAM, Flash, etc.) and will take
       up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
    {
 
               IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
 
    }
    */
 
   /* .reset is a standard section used by the compiler.  It contains the */
   /* the address of the start of _c_int00 for C Code.   /*
   /* When using the boot ROM this section and the CPU vector */
   /* table is not needed.  Thus the default type is set here to  */
   /* DSECT  */
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT
   vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
 
}
 
/*
//===========================================================================
// End of file.
//===========================================================================
*/

 

  • I found the problem if it can help
    I wrote in the CMD file

    .text : > FLASHA | FLASHC | FLASHD, PAGE = 0

    instead of writing

    .text : > > FLASHA | FLASHC | FLASHD, PAGE = 0


    With :>> memory flash A, C and D will be used. it solved my problem.
  • Is that possible to know the real percentage of flash used by the code in the CPU using CCS5, It will be very helpful ??
  • Ol,

    You can instruct the linker to create a text file which records exactly how much memory is occupied and by what each time the project is linked.  Check the linker settings in the build options for your project in CCS.  After linking you can open and inspect the map file in any text editor and find the information you want.

    More information on the linker and map file is in the Assembly Language Tools Guide (lit. ref. spru513h).

    Regards,

    Richard