Other Parts Discussed in Thread: UNIFLASH
Hello everybody,
We just got the TMDSPLCV3KIT the last week. I'm absolute beginner with this kit and I already have some questions.
Hope someone could help me to become more familiar with.
I'm using the two modules with the same laptop and two different GUI windows:
1)my Zero Configuration GUI version is 2.94. How I can get the lastet one?
2) I'm not able to understand why my G3 PLC Initialization fails? (below the log data)
2015-07-15 15:43:54.2364: Windows Version: Microsoft Windows NT 6.1.7601 Service Pack 1
2015-07-15 15:43:54.2744: Zero Configuration GUI - Version: 2.94
2015-07-15 15:43:54.2854: Command Line Arguments:
c:\program files (x86)\texas instruments\plc application suite\plc_application_suite.exe = set
2015-07-15 15:43:54.8624: Port COM10 is unavailable
2015-07-15 15:43:54.8714: Comm port COM8 opened.
: Baud Rate = 57600
: MessageData Bits = 8
: Stop Bits = One
: Parity = None
: Handshake = None
: RTS Enable= True
2015-07-15 15:43:55.2434: Sending: (0x01) - SystemInformation.Request:
2015-07-15 15:43:56.2245: PLC was not found on Port COM8
2015-07-15 15:43:56.1925: Receiving: (0x01) - SystemInformation:
Firmware Version: Major:7 Minor:2 Revision:1 Build:10
Device Type: G3
Device Mode: Point To Point
Hardware Revision: 0
Diagnostics Port: SCI B
Data Port: SCI B
Coherent Modulation: Off
Tonemask Req Mode: Non Designated
Long Address 0x00 00 00 00 00 00 00 00
2015-07-15 15:43:56.3595: Port COM10 is unavailable
2015-07-15 15:43:56.4425: Comm port COM8 opened.
: Baud Rate = 57600
: MessageData Bits = 8
: Stop Bits = One
: Parity = None
: Handshake = None
: RTS Enable= True
2015-07-15 15:43:57.4445: Sending: (0x01) - SystemInformation.Request:
2015-07-15 15:43:57.4735: Receiving: (0x01) - SystemInformation:
Firmware Version: Major:7 Minor:2 Revision:1 Build:10
Device Type: G3
Device Mode: Point To Point
Hardware Revision: 0
Diagnostics Port: SCI B
Data Port: SCI B
Coherent Modulation: Off
Tonemask Req Mode: Non Designated
Long Address 0x00 00 00 00 00 00 00 00
2015-07-15 15:43:57.5635: Sending: (0x01) - SystemInformation.Request:
2015-07-15 15:43:57.5835: Receiving: (0x01) - SystemInformation:
Firmware Version: Major:7 Minor:2 Revision:1 Build:10
Device Type: G3
Device Mode: Point To Point
Hardware Revision: 0
Diagnostics Port: SCI B
Data Port: SCI B
Coherent Modulation: Off
Tonemask Req Mode: Non Designated
Long Address 0x00 00 00 00 00 00 00 00
2015-07-15 15:43:57.6616: Sending: (0x0C) - Load System Config.Request
Load Port Configuration.Request
Configuration Type: Port Designation
Length: 1
Data Port: SCI B
Diag Port: SCI B
2015-07-15 15:43:57.6846: Receiving: (0x0C) - LoadSystem Config.Reply: Status= Success - 0x0000
2015-07-15 15:43:57.7336: Sending: (0x80) - Link Quality Control.Request:
ControlMask: Disable All
Report Interval (sec): 0
2015-07-15 15:43:57.7586: Receiving: (0x0C) - LoadSystem Config.Reply: Status= Success - 0x0000
2015-07-15 15:43:57.7446: Sending: (0x0C) - Load System Config.Request
Load System Configuration.Request
Configuration Type: System Configuration
Length: 26
Device Mode: Point To Point
2015-07-15 15:43:57.7736: Sending: (0x05) - Shutdown.Request
Reset Type: Soft Reset
2015-07-15 15:43:57.7776: Receiving: (0x05) - Shut Down.Reply: Status= Success - 0x0000
2015-07-15 15:43:59.7957: Sending: (0x01) - SystemInformation.Request:
2015-07-15 15:43:59.8237: Receiving: (0x01) - SystemInformation:
Firmware Version: Major:7 Minor:2 Revision:1 Build:10
Device Type: G3
Device Mode: Point To Point
Hardware Revision: 0
Diagnostics Port: SCI B
Data Port: SCI B
Coherent Modulation: Off
Tonemask Req Mode: Non Designated
Long Address 0x00 00 00 00 00 00 00 00
2015-07-15 15:43:59.8917: Receiving: (0x04) - Set Info.Reply: Status= Success - 0x0000
2015-07-15 15:43:59.8937: Sending: (0x04) - Set Information: Request:
Type: G3 PHY TX
Length: 18
TMR: Non Designated
COH: Off
Band Selection: Cenelec
Modulation: ROBO
TX Level: 32
Tone Mask: 0x17 24 FF FF FF FF 0F 00 00 00 00 00 00 00
2015-07-15 15:43:59.9697: Sending: (0x04) - Set Information: Request:
Type: G3 PHY RX
Length: 18
AGC: On
Gain: 0 dB
ROBO: On
BLI: Off
COH: Off
Band Selection: Cenelec
Tone Mask: 0x17 24 FF FF FF FF 0F 00 00 00 00 00 00 00
2015-07-15 15:43:59.9827: Receiving: (0x04) - Set Info.Reply: Status= Success - 0x0000
2015-07-15 15:44:00.0067: G3 PLC Initialization Failed
3)Why I'm not able to send a msg as well? below the log data:
2015-07-15 15:44:42.9681: Receiving: (0x00) - G3 DataTransfer.Confirmation: - Status= 50CD
NSDU Handler: 0
Confirm Flag: Confirm
Status: 0x50CD
2015-07-15 15:44:42.9741: Error Sending Text: 0x000050CD
2015-07-15 15:44:42.9601: Sending: (0x00) - G3 DataTransfer.Request
NSDU Handle: 0
D-Route: Disabled
SEC: Disabled
QoS: Standard Priority
IPv6 Header:
Next Header: 17
Payload Len: 36
Hop Limit: 8
Source Add: FE80:0000:0000:0000:7455:00FF:FE00:0000
Dest Add: FE80:0000:0000:0000:7455:00FF:FE00:0000
UPD Packet:
Source Port: 0x0000
Dest Port: 0x0000
Length: 36
CRC: 0x0000
Data:
0xA0 AA 00 00 00 00 00 00 01 00 0x00 00 01 00 00 00 01 00 00 00
0x04 00 00 00 63 69 61 6F
2015-07-15 15:44:47.8884: Text message was not delivered
Thanks a lot in advance.
Best regards,
Emilio