This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Anyway to reuse GPIO34 in spite of boot rom?

Expert 1960 points

Hi, we run out of GPIO pins and wondering if we can use GPIO34? It's used by boot rom to determine boot mode (SCI/GetMode etc). But we only boot from Flash. IS there anyway to disable or by-pass this check of GPIO34/37 and go directly to boot from Flash? I know this question is asked before, but hoping that there is some way to re-use GPIO34 if we don't need these other boot options. Please advise. Thanks!