Other Parts Discussed in Thread: LVSERVOMTR, DRV8312
Hello I am working with the 28069 chip on the DRV8312EVM board kit along with the motor provided in the kit. I have been going through the builds and have not been able to get the motor to run smoothly, it either vibrates rapidly or is very janky when spinning. I have been changing the values of Iqref and Vqtest and the speedref, while leaving the other variables the same. I have no idea what the units for these values are. I find the manual to be confusing and not very helpful. Is there someone out there who can maybe put it in simpler terms. Or who has worked through these builds that and gotten the motor running smoothly. Help is appreciated.