I am using ADC_SOC example as a base code. I am now trying to receive data from ADCin02 and ADCin03 at around 10Hz. Looking up in the ADC pdf file. I think I understand that I am looking at ADCCLK. ON page 26 of ADC pdf it says that to change ADCCLK, I have to turn on HISPCLK, ADCTRL3 and ADCTRL1. SYSCLKOUT is default 150 MHz. I turned on all bits, but the minimum ADCCLK I can get is around 150kHz. Can I take this number down to 10Hz. If yes, then how?
Thanks.
Waqqas