Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I would like to preserve some RAM contents after Soft Reset.
I am using watchdog reset as a Soft Reset but RAM contents which i want to prevent get set to '0'.
Is watchdog reset, RESET the whole peripherals of controller including RAM ?(Mentione in reference manual)
Is there any direct assembly command to do soft reset?
I checked with alomost all RAM's present on controller(M0, D1 and GS14), after watchdog reset all RAM's get set to '0'.
Is there any way to prevent RAM contents?
Thanks and Regards,
Gajendra Ghate