Hi,
I have a BLDC motor control application in which there will be a inner rate loop/outer position loop holding the motor at its current position. I have hall sensors available and am currently using standard trapazoidal commutation methods. I am interested in moving to a more sophisticated drive scheme to help minimize noise from PWM switching. The motor is low inductance (around 90uH) and thus the PWM frequency is between 100kHz and 150kHz.
I would like to use the launch XL-F28027F with BoostXL drive EVM kit to experiment with.
Can you tell me if the instaspin solution will:
1. Be a less noisy EMI solution vs trapazoidal drive.
2. Will work holding torque at zero speed?
Thanks,
Mitch