Other Parts Discussed in Thread: UNIFLASH
1) When you build the project in CCS set generation *.hex file of the firmware.
2) Until a time (until the project became big) *.hex file through a third-party boot loader C2Prog.
3) After the project became more (as far as I know didn't catch this moment) *.hex file is sutured to the controller, but the controller after a reset to start the program refuses. (tried to mark all 8-nil sectors in memory manual for firmware)
4) Starting proximally UniFlash slipping him the firmware file but in a format *.out all stitched and the controller normally starts after reset.
Has anyone faced such a problem? May C2prog there is a limit in the free version the size of drilled or hex file in CCS are not always correctly compiled?