Other Parts Discussed in Thread: MOTORWARE
/* --COPYRIGHT--,BSD
* Copyright (c) 2012, LineStream Technologies Incorporated
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the names of Texas Instruments Incorporated, LineStream
* Technologies Incorporated, nor the names of its contributors may be
* used to endorse or promote products derived from this software without
* specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
* --/COPYRIGHT--*/
//! \file solutions/instaspin_motion/src/proj_lab06a.c
//! \brief Designing velocity trajectory changes using the SpinTAC Velocity Profile Generator
//!
//! (C) Copyright 2012, LineStream Technologies, Inc.
//! (C) Copyright 2011, Texas Instruments, Inc.
//! \defgroup PROJ_LAB06a PROJ_LAB06a
//@{
//! \defgroup PROJ_LAB06a_OVERVIEW Project Overview
//!
//! Designing velocity trajectory changes using the SpinTAC Velocity Profile Generator
//!
// **************************************************************************
// the includes
// system includes
#include <math.h>
#include "main.h"
#ifdef FLASH
#pragma CODE_SECTION(mainISR,"ramfuncs");
#endif
// Include header files used in the main function
// **************************************************************************
// the defines
#define LED_BLINK_FREQ_Hz 5
// **************************************************************************
// the globals
uint_least16_t gCounter_updateGlobals = 0;
bool Flag_Latch_softwareUpdate = true;
CTRL_Handle ctrlHandle;
HAL_Handle halHandle;
USER_Params gUserParams;
HAL_PwmData_t gPwmData = {_IQ(0.0), _IQ(0.0), _IQ(0.0)};
HAL_AdcData_t gAdcData;
_iq gMaxCurrentSlope = _IQ(0.0);
#ifdef FAST_ROM_V1p6
CTRL_Obj *controller_obj;
#else
CTRL_Obj ctrl; //v1p7 format
#endif
ST_Obj st_obj;
ST_Handle stHandle;
uint16_t gLEDcnt = 0;
volatile MOTOR_Vars_t gMotorVars = MOTOR_Vars_INIT;
#ifdef FLASH
// Used for running BackGround in flash, and ISR in RAM
extern uint16_t *RamfuncsLoadStart, *RamfuncsLoadEnd, *RamfuncsRunStart;
#endif
#ifdef DRV8301_SPI
// Watch window interface to the 8301 SPI
DRV_SPI_8301_Vars_t gDrvSpi8301Vars;
#endif
_iq gFlux_pu_to_Wb_sf;
_iq gFlux_pu_to_VpHz_sf;
_iq gTorque_Ls_Id_Iq_pu_to_Nm_sf;
_iq gTorque_Flux_Iq_pu_to_Nm_sf;
_iq gPotentiometer = _IQ(0.0);
// **************************************************************************
// the functions
void main(void)
{
uint_least8_t estNumber = 0;
#ifdef FAST_ROM_V1p6
uint_least8_t ctrlNumber = 0;
#endif
// Only used if running from FLASH
// Note that the variable FLASH is defined by the project
#ifdef FLASH
// Copy time critical code and Flash setup code to RAM
// The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart
// symbols are created by the linker. Refer to the linker files.
memCopy((uint16_t *)&RamfuncsLoadStart,(uint16_t *)&RamfuncsLoadEnd,(uint16_t *)&RamfuncsRunStart);
#endif
// initialize the hardware abstraction layer
halHandle = HAL_init(&hal,sizeof(hal));
// check for errors in user parameters
USER_checkForErrors(&gUserParams);
// store user parameter error in global variable
gMotorVars.UserErrorCode = USER_getErrorCode(&gUserParams);
// do not allow code execution if there is a user parameter error
if(gMotorVars.UserErrorCode != USER_ErrorCode_NoError)
{
for(;;)
{
gMotorVars.Flag_enableSys = false;
}
}
// initialize the user parameters
USER_setParams(&gUserParams);
// set the hardware abstraction layer parameters
HAL_setParams(halHandle,&gUserParams);
// initialize the controller
#ifdef FAST_ROM_V1p6
ctrlHandle = CTRL_initCtrl(ctrlNumber, estNumber); //v1p6 format (06xF and 06xM devices)
controller_obj = (CTRL_Obj *)ctrlHandle;
#else
ctrlHandle = CTRL_initCtrl(estNumber,&ctrl,sizeof(ctrl)); //v1p7 format default
#endif
{
CTRL_Version version;
// get the version number
CTRL_getVersion(ctrlHandle,&version);
gMotorVars.CtrlVersion = version;
}
// set the default controller parameters
CTRL_setParams(ctrlHandle,&gUserParams);
// setup faults
HAL_setupFaults(halHandle);
// initialize the interrupt vector table
HAL_initIntVectorTable(halHandle);
// enable the ADC interrupts
HAL_enableAdcInts(halHandle);
// enable global interrupts
HAL_enableGlobalInts(halHandle);
// enable debug interrupts
HAL_enableDebugInt(halHandle);
// disable the PWM
HAL_disablePwm(halHandle);
// initialize the SpinTAC Components
stHandle = ST_init(&st_obj, sizeof(st_obj));
// setup the SpinTAC Components
ST_setupVelCtl(stHandle);
ST_setupVelMove(stHandle);
#ifdef DRV8301_SPI
// turn on the DRV8301 if present
HAL_enableDrv(halHandle);
// initialize the DRV8301 interface
HAL_setupDrvSpi(halHandle,&gDrvSpi8301Vars);
#endif
// enable DC bus compensation
CTRL_setFlag_enableDcBusComp(ctrlHandle, true);
// compute scaling factors for flux and torque calculations
gFlux_pu_to_Wb_sf = USER_computeFlux_pu_to_Wb_sf();
gFlux_pu_to_VpHz_sf = USER_computeFlux_pu_to_VpHz_sf();
gTorque_Ls_Id_Iq_pu_to_Nm_sf = USER_computeTorque_Ls_Id_Iq_pu_to_Nm_sf();
gTorque_Flux_Iq_pu_to_Nm_sf = USER_computeTorque_Flux_Iq_pu_to_Nm_sf();
for(;;)
{
// Waiting for enable system flag to be set
while(!(gMotorVars.Flag_enableSys));
// Dis-able the Library internal PI. Iq has no reference now
CTRL_setFlag_enableSpeedCtrl(ctrlHandle, false);
// loop while the enable system flag is true
while(gMotorVars.Flag_enableSys)
{
CTRL_Obj *obj = (CTRL_Obj *)ctrlHandle;
ST_Obj *stObj = (ST_Obj *)stHandle;
// increment counters
gCounter_updateGlobals++;
// enable/disable the use of motor parameters being loaded from user.h
CTRL_setFlag_enableUserMotorParams(ctrlHandle,gMotorVars.Flag_enableUserParams);
// enable/disable Rs recalibration during motor startup
EST_setFlag_enableRsRecalc(obj->estHandle,gMotorVars.Flag_enableRsRecalc);
// enable/disable automatic calculation of bias values
CTRL_setFlag_enableOffset(ctrlHandle,gMotorVars.Flag_enableOffsetcalc);
if(CTRL_isError(ctrlHandle))
{
// set the enable controller flag to false
CTRL_setFlag_enableCtrl(ctrlHandle,false);
// set the enable system flag to false
gMotorVars.Flag_enableSys = false;
// disable the PWM
HAL_disablePwm(halHandle);
}
else
{
// update the controller state
bool flag_ctrlStateChanged = CTRL_updateState(ctrlHandle);
// enable or disable the control
CTRL_setFlag_enableCtrl(ctrlHandle, gMotorVars.Flag_Run_Identify);
if(flag_ctrlStateChanged)
{
CTRL_State_e ctrlState = CTRL_getState(ctrlHandle);
if(ctrlState == CTRL_State_OffLine)
{
// enable the PWM
HAL_enablePwm(halHandle);
}
else if(ctrlState == CTRL_State_OnLine)
{
if(gMotorVars.Flag_enableOffsetcalc == true)
{
// update the ADC bias values
HAL_updateAdcBias(halHandle);
}
else
{
// set the current bias
HAL_setBias(halHandle,HAL_SensorType_Current,0,_IQ(I_A_offset));
HAL_setBias(halHandle,HAL_SensorType_Current,1,_IQ(I_B_offset));
HAL_setBias(halHandle,HAL_SensorType_Current,2,_IQ(I_C_offset));
// set the voltage bias
HAL_setBias(halHandle,HAL_SensorType_Voltage,0,_IQ(V_A_offset));
HAL_setBias(halHandle,HAL_SensorType_Voltage,1,_IQ(V_B_offset));
HAL_setBias(halHandle,HAL_SensorType_Voltage,2,_IQ(V_C_offset));
}
// Return the bias value for currents
gMotorVars.I_bias.value[0] = HAL_getBias(halHandle,HAL_SensorType_Current,0);
gMotorVars.I_bias.value[1] = HAL_getBias(halHandle,HAL_SensorType_Current,1);
gMotorVars.I_bias.value[2] = HAL_getBias(halHandle,HAL_SensorType_Current,2);
// Return the bias value for voltages
gMotorVars.V_bias.value[0] = HAL_getBias(halHandle,HAL_SensorType_Voltage,0);
gMotorVars.V_bias.value[1] = HAL_getBias(halHandle,HAL_SensorType_Voltage,1);
gMotorVars.V_bias.value[2] = HAL_getBias(halHandle,HAL_SensorType_Voltage,2);
// enable the PWM
HAL_enablePwm(halHandle);
}
else if(ctrlState == CTRL_State_Idle)
{
// disable the PWM
HAL_disablePwm(halHandle);
gMotorVars.Flag_Run_Identify = false;
}
if((CTRL_getFlag_enableUserMotorParams(ctrlHandle) == true) &&
(ctrlState > CTRL_State_Idle) &&
(gMotorVars.CtrlVersion.minor == 6))
{
// call this function to fix 1p6
USER_softwareUpdate1p6(ctrlHandle);
}
}
}
if(EST_isMotorIdentified(obj->estHandle))
{
// set the current ramp
EST_setMaxCurrentSlope_pu(obj->estHandle,gMaxCurrentSlope);
gMotorVars.Flag_MotorIdentified = true;
// set the speed reference
CTRL_setSpd_ref_krpm(ctrlHandle,gMotorVars.SpeedRef_krpm);
// set the speed acceleration
CTRL_setMaxAccel_pu(ctrlHandle,_IQmpy(MAX_ACCEL_KRPMPS_SF,gMotorVars.MaxAccel_krpmps));
// enable the SpinTAC Speed Controller
STVELCTL_setEnable(stObj->velCtlHandle, true);
if(EST_getState(obj->estHandle) != EST_State_OnLine)
{
// if the estimator is not running, place SpinTAC into reset
STVELCTL_setEnable(stObj->velCtlHandle, false);
// if the estimator is not running, set SpinTAC Move start & end velocity to 0
STVELMOVE_setVelocityEnd(stObj->velMoveHandle, _IQ(0.0));
STVELMOVE_setVelocityStart(stObj->velMoveHandle, _IQ(0.0));
}
if(Flag_Latch_softwareUpdate)
{
Flag_Latch_softwareUpdate = false;
USER_calcPIgains(ctrlHandle);
// initialize the watch window kp and ki current values with pre-calculated values
gMotorVars.Kp_Idq = CTRL_getKp(ctrlHandle,CTRL_Type_PID_Id);
gMotorVars.Ki_Idq = CTRL_getKi(ctrlHandle,CTRL_Type_PID_Id);
// initialize the watch window Bw value with the default value
gMotorVars.SpinTAC.VelCtlBw_radps = STVELCTL_getBandwidth_radps(stObj->velCtlHandle);
// initialize the watch window with maximum and minimum Iq reference
gMotorVars.SpinTAC.VelCtlOutputMax_A = _IQmpy(STVELCTL_getOutputMaximum(stObj->velCtlHandle), _IQ(USER_IQ_FULL_SCALE_CURRENT_A));
gMotorVars.SpinTAC.VelCtlOutputMin_A = _IQmpy(STVELCTL_getOutputMinimum(stObj->velCtlHandle), _IQ(USER_IQ_FULL_SCALE_CURRENT_A));
}
}
else
{
Flag_Latch_softwareUpdate = true;
// the estimator sets the maximum current slope during identification
gMaxCurrentSlope = EST_getMaxCurrentSlope_pu(obj->estHandle);
}
// when appropriate, update the global variables
if(gCounter_updateGlobals >= NUM_MAIN_TICKS_FOR_GLOBAL_VARIABLE_UPDATE)
{
// reset the counter
gCounter_updateGlobals = 0;
updateGlobalVariables_motor(ctrlHandle, stHandle);
}
// update Kp and Ki gains
updateKpKiGains(ctrlHandle);
// set the SpinTAC (ST) bandwidth scale
STVELCTL_setBandwidth_radps(stObj->velCtlHandle, gMotorVars.SpinTAC.VelCtlBw_radps);
// set the maximum and minimum values for Iq reference
STVELCTL_setOutputMaximums(stObj->velCtlHandle, _IQmpy(gMotorVars.SpinTAC.VelCtlOutputMax_A, _IQ(1.0/USER_IQ_FULL_SCALE_CURRENT_A)), _IQmpy(gMotorVars.SpinTAC.VelCtlOutputMin_A, _IQ(1.0/USER_IQ_FULL_SCALE_CURRENT_A)));
// enable/disable the forced angle
EST_setFlag_enableForceAngle(obj->estHandle,gMotorVars.Flag_enableForceAngle);
// enable or disable power warp
CTRL_setFlag_enablePowerWarp(ctrlHandle,gMotorVars.Flag_enablePowerWarp);
#ifdef DRV8301_SPI
HAL_writeDrvData(halHandle,&gDrvSpi8301Vars);
HAL_readDrvData(halHandle,&gDrvSpi8301Vars);
#endif
} // end of while(gFlag_enableSys) loop
// disable the PWM
HAL_disablePwm(halHandle);
// set the default controller parameters (Reset the control to re-identify the motor)
CTRL_setParams(ctrlHandle,&gUserParams);
gMotorVars.Flag_Run_Identify = false;
// setup the SpinTAC Components
ST_setupVelCtl(stHandle);
ST_setupVelMove(stHandle);
} // end of for(;;) loop
} // end of main() function
interrupt void mainISR(void)
{
static uint16_t stCnt = 0;
// toggle status LED
if(gLEDcnt++ > (uint_least32_t)(USER_ISR_FREQ_Hz / LED_BLINK_FREQ_Hz))
{
HAL_toggleLed(halHandle,(GPIO_Number_e)HAL_Gpio_LED2);
gLEDcnt = 0;
}
// acknowledge the ADC interrupt
HAL_acqAdcInt(halHandle,ADC_IntNumber_1);
// convert the ADC data
HAL_readAdcData(halHandle,&gAdcData);
// Run the SpinTAC Components
if(stCnt++ >= ISR_TICKS_PER_SPINTAC_TICK) {
ST_runVelMove(stHandle, ctrlHandle);
ST_runVelCtl(stHandle, ctrlHandle);
stCnt = 1;
}
// run the controller
CTRL_run(ctrlHandle,halHandle,&gAdcData,&gPwmData);
// write the PWM compare values
HAL_writePwmData(halHandle,&gPwmData);
// setup the controller
CTRL_setup(ctrlHandle);
gPotentiometer = HAL_readPotentiometerData(halHandle);
return;
} // end of mainISR() function
void updateGlobalVariables_motor(CTRL_Handle handle, ST_Handle sthandle)
{
CTRL_Obj *obj = (CTRL_Obj *)handle;
ST_Obj *stObj = (ST_Obj *)sthandle;
gMotorVars.SpeedRef_krpm = gPotentiometer;
// get the speed estimate
gMotorVars.Speed_krpm = EST_getSpeed_krpm(obj->estHandle);
// get the real time speed reference coming out of the speed trajectory generator
gMotorVars.SpeedTraj_krpm = _IQmpy(STVELMOVE_getVelocityReference(stObj->velMoveHandle),EST_get_pu_to_krpm_sf(obj->estHandle));
// get the torque estimate
gMotorVars.Torque_Nm = USER_computeTorque_Nm(handle, gTorque_Flux_Iq_pu_to_Nm_sf, gTorque_Ls_Id_Iq_pu_to_Nm_sf);
// get the magnetizing current
gMotorVars.MagnCurr_A = EST_getIdRated(obj->estHandle);
// get the rotor resistance
gMotorVars.Rr_Ohm = EST_getRr_Ohm(obj->estHandle);
// get the stator resistance
gMotorVars.Rs_Ohm = EST_getRs_Ohm(obj->estHandle);
// get the stator inductance in the direct coordinate direction
gMotorVars.Lsd_H = EST_getLs_d_H(obj->estHandle);
// get the stator inductance in the quadrature coordinate direction
gMotorVars.Lsq_H = EST_getLs_q_H(obj->estHandle);
// get the flux in V/Hz in floating point
gMotorVars.Flux_VpHz = EST_getFlux_VpHz(obj->estHandle);
// get the flux in Wb in fixed point
gMotorVars.Flux_Wb = USER_computeFlux(handle, gFlux_pu_to_Wb_sf);
// get the controller state
gMotorVars.CtrlState = CTRL_getState(handle);
// get the estimator state
gMotorVars.EstState = EST_getState(obj->estHandle);
// Get the DC buss voltage
gMotorVars.VdcBus_kV = _IQmpy(gAdcData.dcBus,_IQ(USER_IQ_FULL_SCALE_VOLTAGE_V/1000.0));
// get the Iq reference from the speed controller
gMotorVars.IqRef_A = _IQmpy(STVELCTL_getTorqueReference(stObj->velCtlHandle), _IQ(USER_IQ_FULL_SCALE_CURRENT_A));
// gets the Velocity Controller status
gMotorVars.SpinTAC.VelCtlStatus = STVELCTL_getStatus(stObj->velCtlHandle);
// get the inertia setting
gMotorVars.SpinTAC.InertiaEstimate_Aperkrpm = _IQmpy(STVELCTL_getInertia(stObj->velCtlHandle), _IQ(ST_SPEED_PU_PER_KRPM * USER_IQ_FULL_SCALE_CURRENT_A));
// get the friction setting
gMotorVars.SpinTAC.FrictionEstimate_Aperkrpm = _IQmpy(STVELCTL_getFriction(stObj->velCtlHandle), _IQ(ST_SPEED_PU_PER_KRPM * USER_IQ_FULL_SCALE_CURRENT_A));
// get the Velocity Controller error
gMotorVars.SpinTAC.VelCtlErrorID = STVELCTL_getErrorID(stObj->velCtlHandle);
// get the Velocity Move status
gMotorVars.SpinTAC.VelMoveStatus = STVELMOVE_getStatus(stObj->velMoveHandle);
// get the Velocity Move profile time
gMotorVars.SpinTAC.VelMoveTime_ticks = STVELMOVE_getProfileTime_tick(stObj->velMoveHandle);
// get the Velocity Move error
gMotorVars.SpinTAC.VelMoveErrorID = STVELMOVE_getErrorID(stObj->velMoveHandle);
return;
} // end of updateGlobalVariables_motor() function
void updateKpKiGains(CTRL_Handle handle)
{
if((gMotorVars.CtrlState == CTRL_State_OnLine) && (gMotorVars.Flag_MotorIdentified == true) && (Flag_Latch_softwareUpdate == false))
{
// set the kp and ki speed values from the watch window
CTRL_setKp(handle,CTRL_Type_PID_spd,gMotorVars.Kp_spd);
CTRL_setKi(handle,CTRL_Type_PID_spd,gMotorVars.Ki_spd);
// set the kp and ki current values for Id and Iq from the watch window
CTRL_setKp(handle,CTRL_Type_PID_Id,gMotorVars.Kp_Idq);
CTRL_setKi(handle,CTRL_Type_PID_Id,gMotorVars.Ki_Idq);
CTRL_setKp(handle,CTRL_Type_PID_Iq,gMotorVars.Kp_Idq);
CTRL_setKi(handle,CTRL_Type_PID_Iq,gMotorVars.Ki_Idq);
}
return;
} // end of updateKpKiGains() function
void ST_runVelMove(ST_Handle handle, CTRL_Handle ctrlHandle)
{
ST_Obj *stObj = (ST_Obj *)handle;
CTRL_Obj *ctrlObj = (CTRL_Obj *)ctrlHandle;
// Run SpinTAC Move
// If we are not in reset, and the SpeedRef_krpm has been modified
if((EST_getState(ctrlObj->estHandle) == EST_State_OnLine) && (_IQmpy(gMotorVars.SpeedRef_krpm, _IQ(ST_SPEED_PU_PER_KRPM)) != STVELMOVE_getVelocityEnd(stObj->velMoveHandle))) {
// Get the configuration for SpinTAC Move
STVELMOVE_setCurveType(stObj->velMoveHandle, gMotorVars.SpinTAC.VelMoveCurveType);
STVELMOVE_setVelocityEnd(stObj->velMoveHandle, _IQmpy(gMotorVars.SpeedRef_krpm, _IQ(ST_SPEED_PU_PER_KRPM)));
STVELMOVE_setAccelerationLimit(stObj->velMoveHandle, _IQmpy(gMotorVars.MaxAccel_krpmps, _IQ(ST_SPEED_PU_PER_KRPM)));
STVELMOVE_setJerkLimit(stObj->velMoveHandle, _IQ20mpy(gMotorVars.MaxJrk_krpmps2, _IQ20(ST_SPEED_PU_PER_KRPM)));
// Enable SpinTAC Move
STVELMOVE_setEnable(stObj->velMoveHandle, true);
// If starting from zero speed, enable ForceAngle, otherwise disable ForceAngle
if(_IQabs(STVELMOVE_getVelocityStart(stObj->velMoveHandle)) < _IQ(ST_MIN_ID_SPEED_PU)) {
EST_setFlag_enableForceAngle(ctrlObj->estHandle, true);
gMotorVars.Flag_enableForceAngle = true;
}
else {
EST_setFlag_enableForceAngle(ctrlObj->estHandle, false);
gMotorVars.Flag_enableForceAngle = false;
}
}
STVELMOVE_run(stObj->velMoveHandle);
}
void ST_runVelCtl(ST_Handle handle, CTRL_Handle ctrlHandle)
{
_iq speedFeedback, iqReference;
ST_Obj *stObj = (ST_Obj *)handle;
CTRL_Obj *ctrlObj = (CTRL_Obj *)ctrlHandle;
// Get the mechanical speed in pu
speedFeedback = EST_getFm_pu(ctrlObj->estHandle);
// Run the SpinTAC Controller
STVELCTL_setVelocityReference(stObj->velCtlHandle, STVELMOVE_getVelocityReference(stObj->velMoveHandle));
STVELCTL_setAccelerationReference(stObj->velCtlHandle, STVELMOVE_getAccelerationReference(stObj->velMoveHandle));
STVELCTL_setVelocityFeedback(stObj->velCtlHandle, speedFeedback);
STVELCTL_run(stObj->velCtlHandle);
// select SpinTAC Velocity Controller
iqReference = STVELCTL_getTorqueReference(stObj->velCtlHandle);
// Set the Iq reference that came out of SpinTAC Velocity Control
CTRL_setIq_ref_pu(ctrlHandle, iqReference);
}
//@} //defgroup
// end of file
After working through the labs, I decided to try using the onboard potentiometer to control the speed of my motor. Following the motorware HAL tutorial, I was able to get the potentiometer to show in the watch expressions window no problem. Now getting it to interface with the motor is a bit tricky! The change that I made was adding the gPotentiometer value within the if(EST_isMotorIdentified(obj->estHandle)) construct :
// set the speed reference
CTRL_setSpd_ref_krpm(ctrlHandle,gMotorVars.SpeedRef_krpm = gPotentiometer);
Even though the SpeedRef_krpm expression in the watch window shows the correct values to make it run (0 - 1.0), the motor very slowly oscillates in place or it might very slowly speed up to the reference value. Is there any reason what would be slowing this down? The ADC conversion seems to work beautifully but when passing those values to the motor, the motor doesn't want to play nice. I attached my project file at the top.
I should mention that the tutorial assumes the user is using lab 3a, but I wanted to take advantage of SpinTac velocity control and Move, hence lab 6a.
Cheers,
Jim