Other Parts Discussed in Thread: CONTROLSUITE, TMS320F28035
Hi all,
I tried to use CLAsin and CLAcos functions in CLA program but I got problem.
When I use this functions, some errors are occur on as flowing description.
#10010 errors encountered during linking; "UPS_FLASH.out" not built C/C++ Problem
#16008-D file "../CLAmath_fpu32.lib<CLAcos.obj>" specifies ISA revision C/C++ Problem
#16008-D file "../CLAmath_fpu32.lib<CLASinCosTable.obj>" specifies ISA C/C++ Problem
#16008-D file "../IQmath.lib<IQ15div.obj>" specifies ISA revision C/C++ Problem
#16008-D file "../IQmath.lib<IQ24toF.obj>" specifies ISA revision C/C++ Problem
#16008-D file "../IQmath.lib<IQmathTables.obj>" specifies ISA revision C/C++ Problem
#16008-D file "../rts2800_ml.lib<_lock.obj>" specifies ISA revision C/C++ Problem
#16008-D file "../rts2800_ml.lib<args_main.obj>" specifies ISA revision C/C++ Problem
#16008-D file "../rts2800_ml.lib<boot.obj>" specifies ISA revision C/C++ Problem
#16008-D file "../rts2800_ml.lib<exit.obj>" specifies ISA revision C/C++ Problem\
#16008-D file "../rts2800_ml.lib<u_tofs.obj>" specifies ISA revision C/C++ Problem
#16008-D file "./source_files/ADC_config/ADC_CONFIG.obj" specifies ISA C/C++ Problem
#16008-D file "./source_files/Function_and_init_files/CLAdiv.obj" C/C++ Problem
#16008-D file "./source_files/Function_and_init_files/CLAsqrt.obj" C/C++ Problem
#16008-D file "./source_files/Function_and_init_files/DSP2803x_ECan.obj" C/C++ Problem
#16008-D file "./source_files/Function_and_init_files/EEPROM.obj" C/C++ Problem
#16008-D file "./source_files/task_files/CLA-Tasks_C.obj" specifies ISA C/C++ Problem
I also use CLAdiv function and it is so good.
"CLAmath.h" was incluced,
in CMD_files:
CLAmathTables : > CLARAM1, PAGE = 1
CLA1mathTables : > CLARAM1, PAGE = 1
Could you tell me the way to fix it.
Thank you!