Other Parts Discussed in Thread: CONTROLSUITE
_F28x_usDelay works in Debug mode but not in Release mode.
I am using the F2837xD source files in controlSUITE and an example project.
In F2837xD_Examples.h there is a DELAY_US defined and I am using that in the main code.
In release mode when the software gets to the delay assembly function (F2837xD_usDelay.asm) the debugger stops and says "No source available for 0x3fe493" and the disassembly shows a "ESTOP0" assembly command. The program works up to the delay assembly code.
I looked closer and there is a C2000 assembly command SB called with a zero offset and a conditional code of unconditional. I think this means the same as while(1) in c code. Isnt it branching to the same line forever?
Is there a workaround? I just need a delay function without creating it myself. Thanks.