This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Insta-Spin lab 4 no output current



Can anyone give me a hint as why my motor inverter does not respond to the IqRef command in lab 4. The motor, code, and inverter all work in fine in lab 3b, but when I go to lab4 I get 0 current out of the inverter no matter what value of Iq I command. I compiled the code, generated the .out file, brought up the lab4 js file, set to real time, hit run and refresh. then I set Flag_enableSys and Flag_Run_Identify to true. I change the Iq reference from 0.1 to 2 A and no current output appears on the scope. I am monitoring the a phase leg to the motor. I have tried three different motors and all exhibit the same issue -no output current from the bridge. Where should I start trouble shooting?

Thanks,

Chuck