Does anyone know how to save the projects in the Motorware labs to another name without causing CCS to crash? I had an instance where I wanted to see if some code I added to a project was causing a problem. I needed to see if it was a hardware or software issue. So I saved the code of Lab 05b to Potentiometer. CCS did not like that at all. Before even compiling I had 55 errors and the folder disappeared when I restarted CCS. I had start completely over with a new set of projects. How can I save a project to a different name and then import a clean project from the working directory?
-Chuck