Other Parts Discussed in Thread: TLK110
I have had two TMDSCNCD28M36 Control Cards installed in an instrument (custom daughter board interface) in which the Ethernet connection just stopped working. Once I plug a cable into the port the lights simply turn off. has anyone else seen this issue? Is there any value in sending these back to TI for investigation? We use these control cards in a 10 custom applications and are becoming concerned. The serial numbers are 1210030 and 1210059 if that helps with any diagnostics. The Ethernet is connected to a host PC using a Belkin USB 2.0 to Ethernet adapter. Other questions are welcome.