Other Parts Discussed in Thread: CONTROLSUITE
Hello
I am using the McBSP in SPI master mode on my F28067, in my SPI communication I have to control one sensor.
The message sent perfectly, CLKX, DX DR and FSX are good. (verify to oscilloscope)
but I don't understand, I've sent Dx normaly and the sensor operates, yet in the DR register I can't write good data, in Dr I receive the Dx register.
Could you help me ?
Thanks in advance.
void init_dma()
{
EALLOW;
DmaRegs.DMACTRL.bit.HARDRESET = 1;
__asm(" NOP"); // Only 1 NOP needed per Design
DmaRegs.CH1.MODE.bit.CHINTE = 0;
// Channel 1, McBSPA transmit
DmaRegs.CH1.BURST_SIZE.all = 0; // 1 word/burst
DmaRegs.CH1.SRC_BURST_STEP = 0; // no effect when using 1 word/burst
DmaRegs.CH1.DST_BURST_STEP = 0; // no effect when using 1 word/burst
DmaRegs.CH1.TRANSFER_SIZE = 127; // Interrupt every frame (127 bursts/transfer)
DmaRegs.CH1.SRC_TRANSFER_STEP = 1; // Move to next word in buffer after each word in a burst
DmaRegs.CH1.DST_TRANSFER_STEP = 0; // Don't move destination address
DmaRegs.CH1.SRC_ADDR_SHADOW = (Uint32) &Sdata[0]; // Start address = buffer
DmaRegs.CH1.SRC_BEG_ADDR_SHADOW = (Uint32) &Sdata[0]; // Not needed unless using wrap function
DmaRegs.CH1.DST_ADDR_SHADOW = (Uint32) &McbspaRegs.DXR1.all; // Start address = McBSPA DXR
DmaRegs.CH1.DST_BEG_ADDR_SHADOW = (Uint32) &McbspaRegs.DXR1.all; // Not needed unless using wrap function
DmaRegs.CH1.CONTROL.bit.PERINTCLR = 1; // Clear peripheral interrupt event flag
DmaRegs.CH1.CONTROL.bit.ERRCLR = 1; // Clear sync error flag
DmaRegs.CH1.DST_WRAP_SIZE = 0xFFFF; // Put to maximum - don't want destination wrap
DmaRegs.CH1.SRC_WRAP_SIZE = 0xFFFF; // Put to maximum - don't want source wrap
DmaRegs.CH1.MODE.bit.CHINTE = 1; // Enable channel interrupt
DmaRegs.CH1.MODE.bit.CHINTMODE = 1; // Interrupt at end of transfer
DmaRegs.CH1.MODE.bit.PERINTE = 1; // Enable peripheral interrupt event
DmaRegs.CH1.MODE.bit.PERINTSEL = DMA_MXEVTA; // Peripheral interrupt select = McBSP 0A
DmaRegs.CH1.CONTROL.bit.PERINTCLR = 1; // Clear any spurious interrupt flags
// Channel 2, McBSPA Receive
DmaRegs.CH2.MODE.bit.CHINTE = 0;
DmaRegs.CH2.BURST_SIZE.all = 0; // 1 word/burst
DmaRegs.CH2.SRC_BURST_STEP = 0; // no effect when using 1 word/burst
DmaRegs.CH2.DST_BURST_STEP = 0; // no effect when using 1 word/burst
DmaRegs.CH2.TRANSFER_SIZE = 127; // Interrupt every 127 bursts/transfer
DmaRegs.CH2.SRC_TRANSFER_STEP = 0; // Don't move source address
DmaRegs.CH2.DST_TRANSFER_STEP = 1; // Move to next word in buffer after each word in a burst
DmaRegs.CH2.SRC_ADDR_SHADOW = (Uint32) &McbspaRegs.DRR1.all; // Start address = McBSPA DRR
DmaRegs.CH2.SRC_BEG_ADDR_SHADOW = (Uint32) &McbspaRegs.DRR1.all; // Not needed unless using wrap function
DmaRegs.CH2.DST_ADDR_SHADOW = (Uint32) &Rdata[0]; // Start address = Receive buffer (for McBSP-A)
DmaRegs.CH2.DST_BEG_ADDR_SHADOW = (Uint32) &Rdata[0]; // Not needed unless using wrap function
DmaRegs.CH2.CONTROL.bit.PERINTCLR = 1; // Clear peripheral interrupt event flag
DmaRegs.CH2.CONTROL.bit.ERRCLR = 1; // Clear sync error flag
DmaRegs.CH2.DST_WRAP_SIZE = 0xFFFF; // Put to maximum - don't want destination wrap
DmaRegs.CH2.SRC_WRAP_SIZE = 0xFFFF; // Put to maximum - don't want source wrap
DmaRegs.CH2.MODE.bit.CHINTE = 1; // Enable channel interrupt
DmaRegs.CH2.MODE.bit.CHINTMODE = 1; // Interrupt at end of transfer
DmaRegs.CH2.MODE.bit.PERINTE = 1; // Enable peripheral interrupt event
DmaRegs.CH2.MODE.bit.PERINTSEL = DMA_MREVTA; // Peripheral interrupt select = McBSP MRSYNCA
DmaRegs.CH2.CONTROL.bit.PERINTCLR = 1; // Clear any spurious interrupt flags
EDIS;
}