This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about using 28027F and Hvkit to run the motor

Hello,

         I use 28027F and Hvkit to control my induction motor, I Use the [M3] on the HVMTRKIT baseboard as the simulator and control the motor by ccs.  So I Insert jumper [Main]-J9, Remove jumper [M3]-J5. 

        When I only use the 15V input, debug the lab9a, then test the Pwm1,2,3. And these are ok.

        But then I insert the 220AC input, debug the lab9a. Set the Flag_enableSys equal to 1, and set the Flag_Run_Identify equal to 1. But then the CCS

has no response. I can not click any button on the ccs, and there are some error like that, all the expressions become red and Console has Error-150.

How can I solve it? What wrong with it? Before I use 28027F, I use the 28069M to control motor, everything is OK.