This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

External ADC for use with eZdsp f28335



I have eZdsp f28335 but unfortunately ADC channels are broken, so i decided to use an external ADC that can outputs serial data

(it has 4 ports - 1 pin for 1 serial port)

Can I connect the output of the ADC (serial) to  a Digital input of the DSP?

or what can i do?