Hi,
I installed the CCSv6 and Control Suite, i connect the LaunchPad and the temperature program runs, I can see the data on the screen of a terminal. Also in the system device driver this is XDS100 COM6.
Now I open the Example_2806xGPIOSetup project, this compiles but does not debug, I get the following error message appears.
Error connecting to the target:
(Error -1135 @ 0x0)
The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 5.1.641.0)
I opened other projects in this folder but i can not communicate with the launchpad. What will be missing me?
help please
thanks
Renato