I have an analog +-10V signal that needs to be input to an ADC channel on TMS320F2837xD Delfino. I will scale the signal to +-5V, which I think is the voltage limit on the ADC pin. Do I need to provide inputs to VrefHi and VrefLo pins also or can I get away with just making sure the signal is in the 0-5V range?