Hello chris
I found another issue: when I use GPIO 29 to connect data line of temperature sensor 18B20 with single-bus architecture,found I can not setup timing sequence successfully.So I did a test,I only set GPIO29 high level at the beginning of interrupt,then I use oscilloscope to survey wave of GPIO29 in lab01.
setting about Hal.c
setting about lproj_lab01.c
At last, I found when execute the function "HAL_setGpioHigh(halHandle,GPIO_Number_29)" the first time,GPIO29 will turn low level about 100ns. This issue make timing sequence chaotic.