Hi, I have some questions concerning the data structures and and variables used in Motorware and Universal GUI.
1). In the InstalSPIN_F28066xM_UNIVERSAL GUI on the "FOC" tab, is the field labelled "Flux (V/Hz)" correspond with the gMotoVar.FluxVpHz and is the unit for both Voltage per Hz?
2). What is the difference between gMotoVar.FluxVpHz and gMotoVar.FluxWb?
3). Is there a suggested document where I can read about what each of the member variables of the gMotoVar structure mean?
4). I noticed some of the member variables in gMotoVar structure are not in engineering units. For example, the member variables having to do with speed such as gMotoVar.Speed_krpm is not in KRPM. What unit is it in and how do I convert it to KRPM?
Thanks in advance.