This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

After CCS crashes - workspace is locked?



Hi folks,

I must be doing something wrong or I just have an exceptionally flaky PC but every so often I manage to crash the CCS program. Once that happens I can't just close it and re-open it because when I do it gives me an error saying that "the workspace is still in use and please select another one".  Is there a workaround to this issue? 

I'm using win7 and it normally is quite stable.  Is there a file I can erase that would allow CCS to load the default workspace as usual?  Or am I stuck in having to reboot the PC?


Thanks,

Richard