Hallo to everybody,
i would like to set 2 questions.
I created a programm in Matlab Simulink and with the CCS i run it to my C2000 piccolo launchpad.
1) How can i power the microcontroller , so that it runs the programm without being connected to the pc (via USB)
2)How can i burn the programm in the C2000, so that it does not run only when the Launchpad is connected with the PC and when CCS is running
Thank you in advance for your support