Other Parts Discussed in Thread: TMS320F28335
Dear sir,
I am establishing the communication between 2 TMS320F28335 DSP'S through DUAL PORT RAM(IDT70V24S20PFI) using external interface. When I am Read/write on the right side of DPRAM, it is working good. But when I am writing on the left side of DPRAM if I Write interger 40 in DPRAM Location it is writing 0xFF in DPRAM Location, it is 16bit DPRAM and I am I have configured the necessary GPIOS as Address lines and Data lines. I am unable to findout the problem.