I import the example project(ADC SOC(C28x)) into CCSv6.1.0 from controlSUITE, and the project can build successfully.
But when I want to burn-in TMS320F28035, the project can not build. I have added DSP2803x_Memcopy.c file to the project, defined extern variables above main() function and replaced 28035_RAM_lnk.cmd with F28035.cmd.
I also want to consult why DSP2803x_Memcopy.c file is not found in C:\ti\controlSUITE\device_support\f2803x\v130\DSP2803x_common\source.
so I used the DSP2803x_Memcopy.c file in v125. Is it a problem that cause the compilation failure?
Could you please give me some advice about that?
Thanks a lot.